Adding Motion
There are two ways to create motion, depending on the motion engine:
- For Pipe Network, refer to Design Motion with Pipe Network
- For PLCopen
A vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML, refer to Design Motion with PLCopen Axis - If you are not sure which engine to use, refer to Pipe Network or PLCopen
For high-level discussions about
|
Copyright © 2018 Kollmorgen |
|